-- S T O L L M A N N   E & V   G M B H --
                                                                   [13.06.2013]

Releasenotes for Stollmann NFCStack+Eva TI R6.0.57.5
=====================================================

Changes:
--------
- NFCStack+Eva TI: Remove Card Emulation in secure elements column and associated tab (10221)

Fixed bugs:
-----------
- none

Known  Issues:
--------------
- write large ndef messages to type 2 tags fails (8458)
- NFCPlayer: transferred picture via SNEP is not shown in NFCPlayer (8389)
- Using CardEmulation, a reconnect requires a restart of the listeners
- NDEF functions do not encode strings into UTF-8 encoding. All content
  is handled transparent. (5165)
- Tag type 4 tags being removed from the reader can block the further 
  detection for 20 seconds. This is due to the recovery procedures of 
  type 4 tags. (5028)


Releasenotes for Stollmann NFCStack+Eva TI R6.0.55.5
=====================================================

Changes:
--------
- NFCStack+Dev/Eva TI: Install directory now C:\TI (10192)
- NFCPlayer: set correct component number for STOLLMANN_PRODUCT_DEVKIT_TI (10185)
- NFCPlayer: Remove the handover server from the P2P Tab
- NFCPlayer: Changed the text "Low speed" to 6.7 kbit/s

Fixed bugs:
-----------
- If the NFCC sends a DEACTIVATE_NTF with the Parameter DISCOVERY_MODE in 
  listenSleep then the transition to this state is missing. (10200)

Known  Issues:
--------------
- write large ndef messages to type 2 tags fails (8458)
- NFCPlayer: transferred picture via SNEP is not shown in NFCPlayer (8389)
- Using CardEmulation, a reconnect requires a restart of the listeners
- NDEF functions do not encode strings into UTF-8 encoding. All content
  is handled transparent. (5165)
- Tag type 4 tags being removed from the reader can block the further 
  detection for 20 seconds. This is due to the recovery procedures of 
  type 4 tags. (5028)


Releasenotes for Stollmann NFCStack+Eva TI R6.0.51.5
====================================================

Changes:
--------
- nfcSecureSetTimeout and nfcSecureGetRoutingEntries not exported (10140)
- Add bitrate setting for TAG polling (9836)
- NFaCe+SPASpecification must be updated for NFCStack r16.0.x.y (10098)

Fixed bugs:
-----------
- nfcPlayer crashes in CE mode when printing large data to debugout (10139)
- NCI Stack cannot work with TI ISO 15693 tags on TI chip (9860)
- SAK value: neglect not relevant bits from SEL_RES (9727)
- P2P using NCI: chained data not handled correctly
- NFCPlayer: Function of "presence check" does not work correctly (8456)

Known  Issues:
--------------
- write large ndef messages to type 2 tags fails (8458)
- NFCPlayer: transferred picture via SNEP is not shown in NFCPlayer (8389)
- Using CardEmulation, a reconnect requires a restart of the listeners
- NDEF functions do not encode strings into UTF-8 encoding. All content
  is handled transparent. (5165)
- Tag type 4 tags being removed from the reader can block the further 
  detection for 20 seconds. This is due to the recovery procedures of 
  type 4 tags. (5028)


Releasenotes for Stollmann NFCStack+Eva TI R6.0.47.5
====================================================

Changes:
--------
- NFCPlayer: make dialogs modal (9939)
- RW/CE: nfcman nfcGetTagInfo causes stack failure (9824)

Fixed bugs:
-----------
- calculated bit rate out of values from activated ntf is wrong if bitrate is higher than 848kBit/s (10106)
- NFCPlayer: crashes if trace flags dialog was opened from controller dialog (9940)
- Chip crash leaves stack in undefined state (9261)
- Handover client send EV_CONNECT twice (9210)

Known  Issues:
--------------
- NFaCe+SPASpecification must be updated for NFCStack r16.0.x.y (10098)
- NCI Stack cannot work with TI ISO 16693 tags on TI chip (9860)
- write large ndef messages to type 2 tags fails (8458)
- NFCPlayer: Function of "presence check" does not work correctly (8456)
- NFCPlayer: transferred picture via SNEP is not shown in NFCPlayer (8389)
- Using CardEmulation, a reconnect requires a restart of the listeners
- NDEF functions do not encode strings into UTF-8 encoding. All content
  is handled transparent. (5165)
- Tag type 4 tags being removed from the reader can block the further 
  detection for 20 seconds. This is due to the recovery procedures of 
  type 4 tags. (5028)


Releasenotes for Stollmann NFCStack+Eva TI R6.0.44.5
=============================================================

Changes:
--------
- raised major version number, e.g. show official support for NCI

Fixed bugs:
-----------
- For TRF7970 is Felica CE in supported listen mask
- NfcPlayer: crash after installation when used config button from card emulation tab (9986)
- NfcPlayer: cannot find his INI file when called like "c:\windows\nfcplayer.exe" (9985)

Known  Issues:
--------------
- NCI Stack cannot work with TI ISO 16693 tags on TI chip (9860)
- write large ndef messages to type 2 tags fails (8458)
- NFCPlayer: Function of "presence check" does not work correctly (8456)
- NFCPlayer: transferred picture via SNEP is not shown in NFCPlayer (8389)
- Using CardEmulation, a reconnect requires a restart of the listeners


Releasenotes for Stollmann NFCStack+Eva TI R5.1.42.5
=============================================================

Changes:
--------
- NFCPlayer: added TI logo and default configuration for TI reader TRF7970
- NFCPlayer: make dialogs modal (9939)
- Bitrate for 14443/Felica/15693 configurable in ListenReq when using NCI

Fixed bugs:
-----------
- NFCPlayer: crashes if trace flags dialog was opened from controller dialog (9940)

Known  Issues:
--------------
- write large ndef messages to type 2 tags fails (8458)
- NFCPlayer: Function of "presence check" does not work correctly (8456)
- NFCPlayer: transferred picture via SNEP is not shown in NFCPlayer (8389)
- Using CardEmulation, a reconnect requires a restart of the listeners